Technical FAQs

Ask a Question

When we use IEC61850 driver in Vijeo Citect then what is the maximum allowable IED/ICD files that we can configure.

There is no such limitation of configuring the IED/ICD file in Vijeo Citect as you have the options to configure more IO Servers to communicate with devices on IEC61850.
Was this helpful?
What can we do to improve the information ?