Technical FAQs

Ask a Question

Is cascading of the Reflex iC60 identical to that of an iC60 circuit breaker.

Yes, the cascading of the Reflex iC60 identical to that of an iC60 circuit breaker.
Was this helpful?
What can we do to improve the information ?