Technical FAQs

Ask a Question

What will happen if someone reset the operating handle of Reflex iC60 and the short-circuit fault is still present.

If someone reset the operating handle of Reflex iC60 and the short-circuit fault is still present then self-tripping occurs upon closing of the contacts and the operating handle returns to opening position.
Was this helpful?
What can we do to improve the information ?