Technical FAQs

Ask a Question

What will happen if the test button of the Vigi associated with the Reflex iC60 is actuated.

When the test button of the Vigi associated with the Reflex iC60 is actuated then this opens the power circuit of the Reflex iC60 to go into disconnection position and the indicator on the front is lit flashing orange.
Was this helpful?
What can we do to improve the information ?