Technical FAQs

Ask a Question

What is the maximum length of the control cable allowed for inputs Y1, Y2 and Y3 of Reflex iC60.

The maximum length of the control wires for inputs Y1 and Y2 at a voltage of 230 Vac is:
- 100 metres if a cable is used;
- 500 metres if wires in an electrical duct are used.
The maximum length of the control wires for the Y3 input at a voltage of 230 V DC/AC is 500 m.
Was this helpful?
What can we do to improve the information ?