Technical FAQs

Ask a Question

Is there any remote status indication available in Reflex iC60.

The Reflex iC60 has two dry contacts, O/C and Auto/OFF. The O/C contact indicates the position of the contacts (opened or closed).
The Auto/OFF contact indicates the position of the circuit breaker's operating handle: in Auto position, the operating handle is closed, the contacts are operational.
In OFF position, the operating handle is open, the circuit breaker is disconnected, and the contacts are therefore non-operational.
Was this helpful?
What can we do to improve the information ?