Technical FAQs

Ask a Question

Why we get the error while installing Vijeo Desiner from installation DVD. The error is "Error 1324: The path contains an invalid characters".

This installation problem is because of the system Locale set to other than english where the path specifier in windows is different than "/".
Set the system locale to English and then install the software and then after the installation set back the system locale to previous Local will solve the problem.

To change the system Locale:
1. Open control panel.
2. Select Region and Language.
3. In Region and Language go to Administrative Tab and click on Change System Locale.
4. Select System Locale and clock ok to apply.
5. After Changing the System Locale you need to restart the System to apply new settings.
Was this helpful?
What can we do to improve the information ?