Technical FAQs

Ask a Question

How to find cross reference of a Variable in Vijeo Designer to check where it has been used.

There is no Find function available in Vijeo Designer to simply search for the variable and its cross reference. 

To check the cross reference a variable in Vijeo Designer that where it has been used you need to generate variable report. To do this: 

1. On the Navigator window right click on Variable. 
2. Select the Option Variable Reference & Reports.. 
3. It will ask to validate your target. Simply press yes. 
4. Now one window will appear as Select a Report. 
5. In Available Report drop-down choose the option "Cross Reference all variables by Name" and press ok button. 
6. This will generate a variable list with address and references. All the variables and references are having a hyperlink which means that you can directly go to the reference by clicking on them and it will automatically direct you to that object. 
Was this helpful?
What can we do to improve the information ?