Technical FAQs

Ask a Question

PM5560 auxillary/control power supply ranges from 100-480VAC is this V LN or V LL.

As per specification's in installation guide control power AC: 100 to 480 V L-N ± 10% (refer page 7/18).
Was this helpful?
What can we do to improve the information ?