Technical FAQs

Ask a Question

​What is the difference between LV434010 & LV434011 IFE interface.

There are 2 commercial references of the IFE:
  • LV434010 - Ethernet interface for LV circuit breaker.
    • This type of IFE is an Ethernet interface for Compact, PowerPact, and Masterpact circuit breakers.
  • LV434011 - Ethernet interface for LV circuit breaker and gateway.
    • This type of IFE is an Ethernet interface for Compact, PowerPact, and Masterpact circuit breakers and a gateway for Modbus-SL (serial line) connected devices.
Was this helpful?
What can we do to improve the information ?