Technical FAQs

Ask a Question

What are the main features of IFE Ethernet interface for LV circuit breaker.

The main features of IFE are:
  • Dual Ethernet port for simple daisy chain connection
  • Device profile web service for discovery of the IFE on the local area network (LAN)
  • ULP compliant for localization of the IFE in the switchboard
  • Ethernet interface for Compact, PowerPact, and Masterpact circuit breakers
  • Gateway for Modbus-SL connected devices (only for the IFE with the commercial reference LV434011)
  • Embedded set-up web pages
  • Embedded monitoring web pages
  • Embedded control web pages
  • Built-in e-mail alarm notification
Was this helpful?
What can we do to improve the information ?