Technical FAQs

Ask a Question

What is the main function of TRV00217 stacking accessory and to which LV circuit breaker IFE interface should be used.

The IFE mounts on a DIN rail. The stacking accessory TRV00217 enables the user to connect several IFMs to an IFE
gateway without additional wiring.
NOTE: The stacking feature is available only for the IFE with the commercial reference LV434011.
Was this helpful?
What can we do to improve the information ?