Technical FAQs

Ask a Question

What is the function of IO input/output interface for LV circuit breaker and does it possible to wired to transfer status of some external inputs from different devices.

The IO input/output interface for LV circuit breaker module with several inputs/outputs (6 digital inputs and 3 outputs and one input for temperature sensor), and a rotary switch providing predefined or user-defined applications.

By default, the IO is set with the rotary switch in position one, providing the craddle management application (as per the CCM).
The customer has to wire the contacts CE/CT/CD of the breaker to the 3 inputs ot IO as per the user manual.
3 others inputs are available for customer to assign functions availale by the Electrical Asset Manager software (RSU for instance). Whatever device can be connected by taking into account the electrical features of the IO.
Was this helpful?
What can we do to improve the information ?