Technical FAQs

Ask a Question

Can we configure 2 ports on the ScadaPack 314 RTU as RS-485.

There is no setting of RS485 for SCADA PACK 314 in Telepace Studio but these ports will work as RS485 on the setting of RS232 only .To achieve RS485 functionality on these ports we need to set the Jumper setting(RS232 or RS485) in SCADA PACK RTU itself.
Refer the attached document for SCADA PACK 314 configuration.
Was this helpful?
What can we do to improve the information ?