Technical FAQs

Ask a Question

How can we configure this XMLB070D2S11 sensor so that when minimum pressure reached 30 bar, the contact is switched.

This XMLB070D2S11 is a pressure switch which regulates between two thresholds limits, so you need to set the maximum & minimum pressure settings. Suppose you want to switch the contacts at 30 bars then you can set the PB (min) to 30 bars so that when the pressure goes above 30 bars your contact 13-14 remains as it is (NO) and when this pressure goes to the maximum limit set point (PH) suppose 50 bars then your contacts 13-14 changed to NC and now when this pressure goes down below 30 bars then again these contacts 13-14 changed to NO till it reaches max pressure set limit. 
Was this helpful?
What can we do to improve the information ?