Technical FAQs

Ask a Question

Is it possible to overwrite a output RTF Report file in Vijeo Citect such that I don`t need a append output RTF file.

Yes you can overwrite a RTF file such that you will get only a single report file, but this depend on how you have configure this report & you device which is used in the report output. You have to configured RTF report with device, time, period and No of files field defined. To append a single file only you need to put -1 in the No of file field of the device. It then generates a single report only.
Was this helpful?
What can we do to improve the information ?