Technical FAQs

Ask a Question

In which format the alarm and summary will be logged in Vijeo Citect and how can I log these alarms in Excel file.

These alarms & summary will store in Text files by default if you select the logging device in Alarm Category as "Alarm Disk" or "Summary Disk". 

To log a alarms or Summary in Excel , DBF or CSV format you need to configure a Device in Citect Explorer >> System >> Device. Then you need to use this device in Alarm Category >> Log Device 
Was this helpful?
What can we do to improve the information ?