Technical FAQs

Ask a Question

What is the resistance of Acti9 shunt coil iMX.

The resistance of Acti9 Shunt coil iMX is given below

a) A9A26476 ( 100 .. 415V AC / 110 ... 130V DC ) >> 406 ohm
b) A9A26477 ( 48V AC/DC ) >> 73 ohm 
c) A9A26478 ( 12 ... 24V AC/DC ) >> 4.7 ohm
Was this helpful?
What can we do to improve the information ?