Technical FAQs

Ask a Question

Do we have any momentum module that supports Modbus Plus with Unity Pro.

There is no specific momentum module is available that supports Modbus Plus on Unity Pro. 

To have integration with existing Modbus Plus installation for old Momentum CPU you can begin the process of modernizing from Modbus Plus to Ethernet using the Modbus Plus Proxy Part No. TCSEGDB23F24FA 

• Proxy can continue Modbus Plus Peer Cop and Global Data connectivity to legacy devices on Modbus Plus 
• Unity Momentum can maintain connectivity to both Modbus Plus and Ethernet devices with function code and programming support 
• The Proxy has been tested to support Unity Momentum with existing Proxy firmware v1.0 or higher. 

refer the attached document for your reference 
Was this helpful?
What can we do to improve the information ?