Technical FAQs

Ask a Question

What is the default interval 140CRP31200 module uses to synchronize with NTP server

The default time used by CRP to sync with NTP server is 20s. This time is called polling time interval that would be used to update the crp time,  if you put 50s time would be synced from server every 50s.
Was this helpful?
What can we do to improve the information ?