Technical FAQs

Ask a Question

What is the minimum and maxmum cable size of BCPM/BCPMSC control power and voltage input terminals.

The control and voltage input uses a 2.5 mm² connector, indicated for cables from 24 to 12 AWG.
On the length side, please evaluate the load and specify the cable diameter accordingly.
For the Voltage input the load of the equipment is of maximum 15VA and the fuse indicated for the installation is 500mA.
Was this helpful?
What can we do to improve the information ?