Technical FAQs

Ask a Question

What is the sheet steel composition of Prisma iPM enclosures.

The sheet metal used for Pirsma iPM is DC01, which is cold rolled carbon steel, it complies with EURO standard EN10130. 
Please refer below the chemical composition of DC01.

 
Was this helpful?
What can we do to improve the information ?