Technical FAQs

Ask a Question

What is the syntax of the IP address in a READ_VAR or WRITE_VAR block in Unity Pro with an M340?

The syntax for indicating the IP address of the Modbus TCP/IP device to which the READ_VAR or WRITE_VAR function is to communicate is as follows: ADDM('network_link ') Example: ADDM('Ethernet_1{192.100.200.120}') Illustration:


Was this helpful?
What can we do to improve the information ?