Technical FAQs

Ask a Question

How many Reflex iC60 devices can be powered by a single protection circuit breaker.

At most five Reflex iC60 devices can be installed under the same 10A-C or 16A-B protection circuit breaker.
However, a distinction should be made between applications in which the Reflex iC60 devices are all controlled simultaneously
and applications when the Reflex iC60 devices are controlled in sequence, which allows a greater number of products to be
protected by a given circuit breaker.
Was this helpful?
What can we do to improve the information ?