Technical FAQs

Ask a Question

What is the tolerance of measurement of rated residual operating current Idn of Residual current circuit breakers.

According to the standards IEC/EN 61008 and 61009, the Residual current circuit breakers (RCCB) devices must mandatory trip between Idn/2 and Idn; and this is applicable for all the temperature range.
Was this helpful?
What can we do to improve the information ?