Technical FAQs

Ask a Question

Can I connect the XBTGT dialogue terminals on a Profibus DP bus?

Yes. All XBTGT terminals (apart from the XBTGT series 1000) can be connected to the Profibus DP bus. The XBTGT terminal must however be equipped with an XBTZGPDP extension module (Profibus port for connection to the bus).

Note:  The terminal will be a slave on the Profibus bus. See also:
Was this helpful?
What can we do to improve the information ?