Technical FAQs

Ask a Question

What is the derating for high altitude application for Altivar 12 drive.

Up to 1000 m without derating
1000...3000 m derating the current by 1 % per additional 100 m.
Was this helpful?
What can we do to improve the information ?