Technical FAQs

Ask a Question

What is the surge withstand specification of RM4TA01 measurement and control relay.

Surge withstands specification of RM4TA01:
The RM4TA01 product is complied with IEC61000-4-5 standard (Part 4-5: Testing and measurement techniques - Surge immunity test). 
L1, L2, L3 Test voltage: 
Common mode = 2000V @ 1.2/50us 
Differential mode = 1000V @ 1.2/50us 
Was this helpful?
What can we do to improve the information ?