Technical FAQs

Ask a Question

Is it possible to connect PT100 sensor to an Altistart 48 soft Starter.


PTC input is incompatible with PT100 sensors.
PTC is a specific resistance which value increase greatly with temperature (Positive Temperature Coefficient).
For ATS48, the recommended value of PTC 3x250 ohms at 25°C.
Was this helpful?
What can we do to improve the information ?