Technical FAQs

Ask a Question

What are the various communication standard supported for Premium communication modules i.e. TSXSCY21601,TSXSCY11601 modules and TSXSCP111,112,114 PCMCIA Card.

The link built into the TSX SCY 21601 module complies with communication standards:
  • Uni-Telway
  • Modbus
  • X-Way
The link built into the TSX SCY 11601 module complies with communication standards:
  • Jbus/Modbus
  • X-Way
TSX SCP 111, 112, 114 PCMCIA cards comply with communication standards:
  • Uni-Telway protocols, Modbus
  • PCMCIA
  • X-Way 
Was this helpful?
What can we do to improve the information ?