Technical FAQs

Ask a Question

What is the function of left dip switch on 140NOM21200, can it be used for user interface.

By default left switch on 140NOM is in upward position and has only one condition linked to it as described in below note. It is not possible to have any kind of user interface with this switch. 

User-added image
Was this helpful?
What can we do to improve the information ?