Technical FAQs

Ask a Question

How to enable communication on all devices connected to serial port of Scadapack controller

To enable communication on all the devices connected on the serial port, an address of 0 is to be used on the ADDRE pin of the MBUSCTRL block. An address of 0 will enable/disable communication to every device on the specified port of Scadapack controller.
Was this helpful?
What can we do to improve the information ?