Technical FAQs

Ask a Question

How to configure IO scanning request using BMXNOC0401 module

For BMXNOC0401, Modbus IO scanner functionality is configured inside the device DTM. This can be done by adding a generic modbus device or any specific modubus dtm device under BMXNOC. Then create a request under Request settings page of the slave dtm. Enclosed is complete procedure.
Was this helpful?
What can we do to improve the information ?