Technical FAQs

Ask a Question

When i download my Unity application to the PLC, why the values entered in animation table are lost

Using Unity Pro when you download the PLC program to the plc, the data in animation tables are reset. This is normal behavior. If you want to retain some values in a particular variable then put the fixed values in VALUE section of a variable in the DATA EDITOR or else use MOVE block to put constant data in allocated variables.
Was this helpful?
What can we do to improve the information ?