Technical FAQs

Ask a Question

Why i unable to RUN /STOP OTB NIM module connected with Advantys software

OTB NIM's module offer restricted number of online operations, which are :-

1. Connecting to the physical island
2. Disconnecting to the physical island
3. Downloading the configured data into the island.
4. Uploading the configured data from the island.
5. Changing the connection settings.

There is restrictions of making RUN / STOP from OTB terminal. It must be scanned by a Master after the configuration download in the OTB NIM.
Was this helpful?
What can we do to improve the information ?