Technical FAQs

Ask a Question

What kind of fiber optic cable can be used for the MT-RJ port of 140NOE77101

The MT-RJ port of NOE77101 is Multimode. For the NOE 771 01, you may need an MT-RJ to SC (duplex) multimode fiber optic cable assembly 62.5/125mm. Schneider Electric recommends cable number 490NOC00005 to connect to fiber hubs/switches. The maximum cable segment length for 100BASE-FX multimode cable (1300 nm) is 2 km.
Was this helpful?
What can we do to improve the information ?