Technical FAQs

Ask a Question

Why i am unable to install Advantys configuration software V8.0

This could happen if you have not properly uninstalled previous installation of Advantys. Do the following to ensure complete un installation.

Go to the Control Panel, Add/Remove Programs and remove Advantys if it is in the list. 

Also, open the Registry Editor (regedit) and go to 
HKEY_LocalMachine\Software\Wow6432Node\Schneider Electric and delete the Advantys folder.   OR at path 
[HKEY_LOCAL_MACHINE\SOFTWARE\Schneider Electric\Advantys] in Win 7 32 bit system to earse the registration of advantys

Reboot and reinstall using the 'run as administrator'. option on the setup.exe. 
Was this helpful?
What can we do to improve the information ?