Technical FAQs

Ask a Question

Could you explain how M580 cpu read/write data from M340 cpu over ethernet network

You have to configure generic modbus device in the M580 CPU DTM to read through M340 CPU modbus tcp port. This can be done in the DTM explorer of M580 cpu by adding M340 as a modbus tcp slave and configuring one ioscanning line. Enclosed is a sample aplication to help.
Was this helpful?
What can we do to improve the information ?