Technical FAQs

Ask a Question

How to RUN Unity pro v8 on PC with Windows 8

Unity 8 run on Windows 8 in compatibility mode. To set “Windows 7 compatibility mode” :
After installation of Unity Pro, start  UPWin8.exe. This exe sets Unity Pro exe files (UnityX.exe, CfCatGui.exe, LibsetServer.exe, SETUPEF.exe, LibsetServer.exe)  in the Windows 7 compatibility mode.
      Note :   It works only for "current user".
 Other method is :
·         right click on Unity Pro icon (or UnityX.exe)
·         edit Properties
·         In Folder Compatibility, select “run  this program in windows 7 Compatibility mode
Same operation must be done on following exe files :
·         CfCatGui.exe, LibsetServer.exe, SETUPEF.exe   (available in ..\Program Files\Schneider Electric\Unity Pro)
·         LibsetServer.exe (available in ..\Program Files\Schneider Electric\Unity Pro\LibsetServer)
Was this helpful?
What can we do to improve the information ?