Technical FAQs

Ask a Question

Can i run Unity Pro v8.1 on Windows 8 PC

Unity Pro v8.1 is a update to Unity Pro v8 and is only compatible to run on Windows 8.1, not on 8.0
Was this helpful?
What can we do to improve the information ?