Technical FAQs

Ask a Question

Is Quantum analog module 140AVI03000 compatible to hart signals

140AVI03000 is not hart compatible. Connecting a hart enabled signal to non hart compatible module would influence the input signal due to high frequency signal. The Hart compatible modules like 140 ACI 03 000 have high frequency filter to extract the analog value, which 140 AVI doesn't have. 
Was this helpful?
What can we do to improve the information ?