Technical FAQs

Ask a Question

What are the steps necessary to do Protective a File action in SoMove.

>> Protective a File action is available in SoMove.
Step     Action 
1     Select the File → Project Properties menu in the menu bar. 

In the Properties box: 
Step     Action 
1     Select the Summary tab. 
2     Click the Modify Protection button. 

In the Modify Protection box: 
Step     Action 
1     Select the Read Write option. 
2     Enter a password in the New field. 
3     Confirm the password in the Confirm field. 
4     Click OK 
Was this helpful?
What can we do to improve the information ?