Technical FAQs

Ask a Question

What is the staus indication of Modbus Serial Line Traffic LED of IFE Ethernet interface for LV circuit breaker.

The Modbus serial line traffic yellow LED, indicates that the traffic is being transmitted or received over the Modbus serial line network through the IFE gateway.
The LED is ON during the transmission and reception of the messages. The LED is OFF otherwise.

NOTE: The LED is OFF on IFE without gateway feature (commercial reference LV434010).
Was this helpful?
What can we do to improve the information ?