Technical FAQs

Ask a Question

How to resetting accumulated energy using the display in iEM3100/iEM3200/iEM3300 series energy meters.

The following resets are available, depending on your meter model:
Partial energy
Input metering

Below is the procedure how to resetting accumulated energy using the display;
1. Navigate to the Partial Active E or Partial Reactive E screen. The screen displays the date of the last reset.
2. Press and hold . The Reset screen appears.
3. Press to confirm the reset and enter the meter password when prompted.
NOTE: Regardless of the screen you use to access this reset, accumulations of both Partial Active Energy and the Partial Reactive Energy (if available) are cleared.
Was this helpful?
What can we do to improve the information ?