Technical FAQs

Ask a Question

Does iEM3100/iEM3200/iEM3300 series energy meters display shows date and time below "total energy" parameter display screen.

There is nothing below "total energy", the installation guide “NHA15789” page 7/14 only describe that "each part can be used to show what information", but which not denote all the information can be showed according to the guide, it is only a sketch map. 

The date and time mentioned is "Partial Energy Reset" time, which can be displayed below the "partial energy" page only after resetting "partial energy".  
Was this helpful?
What can we do to improve the information ?