Technical FAQs

Ask a Question

​What is the significance of programmable digital input in PowerLogic Power metering range of products.

The programmable digital input's Can be programmed to:
> Count pulses from other meters (gas, water, etc.)
> Monitor an external status
> Reset the partial energy accumulation and start a
> new period of accumulation

This allows for monitoring of:
> Intrusion (for example, doors opening) or
> equipment status
> Energy usage
Was this helpful?
What can we do to improve the information ?