Technical FAQs

Ask a Question

What is the significance of programmable digital output in PowerLogic Power metering range of products.

The programmable digital outputs can be programmed to:
> be an active energy (kWh) pulse output, with a configurable pulse weight
> Alarm on configurable pickup setpoint

This allows you to:
> Collect pulses from the meter with a Smartlink system, PLC or any basic acquisition system.
> Monitor power levels at a detailed level and to help detect an overload before the circuit breaker trips
Was this helpful?
What can we do to improve the information ?