Technical FAQs

Ask a Question

What is the Rated impulse withstand voltage (Uimp) of EasyPact TVS GZ1E** range of circuit breakers.

The Rated impulse withstand voltage (Uimp) of EasyPact TVS GZ1E** range of circuit breakers is 6kV conforming to IEC 60947-2 standard.
Was this helpful?
What can we do to improve the information ?