Technical FAQs

Ask a Question

What is the Rated insulation voltage (Ui) of EasyPact TVS GZ1E** range of circuit breakers.

The Rated insulation voltage (Ui) of EasyPact TVS GZ1E** range of circuit breakers is 690V Conforming to IEC 60947-2.
Was this helpful?
What can we do to improve the information ?