Technical FAQs

Ask a Question

What is the flame resistance of EasyPact TVS GZ1E** thermal magnetic circuit breakers.

The flame resistance of EasyPact TVS GZ1E** thermal magnetic circuit breakers is 960°C conforming to IEC 60695-2-1 standard.
Was this helpful?
What can we do to improve the information ?